I am getting 10V across C4 capacitor (referring to the application schematic in datasheet). I have connected the circuit as it is in the application schematic (page 26 of datasheet). Only difference is that I have a 0 ohm resistor between IC ground and power ground.
Supply voltage 14.5 V
Voltage at STAT1 = 0.8V
Voltage at STAT2 = 8.8V
Voltage at PG = 8.8V
LED D2 is glowing brightly, but D3 and D4 are dim. I am testing these without the battery or load connected. As soon as I connect the battery, it is drawing a much higher charging current than I have set for.