Hello!
For BQ24253, referencing datasheet SLUSBA1H.pdf, Table 1 - "EN1 and EN2 Truth Table", and Figure 18 - "bq24253 D+/D- and EN1/EN2" flow chart..
What is state of Input current limit (Ilim) before the D+/D- detection algorithm is done? Is the Input Hi-Z? I understand that EN1 and EN2 are ignored until "a change on the status of the EN1 and EN2 occur[s]".
Schematically, I'm planning to have pin Ilim shorted to GND (default 2A), but datasheet says Ilim pin is ignored for USB, so I expect this to not influence the above question.
Also, I'm planning to use /PG pin to pull EN2 low (EN1 has hardwired pull-up to LDO) to make "Externally programmed by ILIM (up to 2.0A)". Is this an ok way to change ENx pin? It seems 'yes' due to statement in ds, "The PG pin will remain high impedance until the detection has completed."
Thanks in advance!
David McRell