Hello to whom it may concern.
The BQ24171 is designed to be cleared when certain conditions are met even if a timer fault occurs.
The data sheet has the following description.
(Datasheet p23)
- 9.3.21 Timer Fault Recovery
The IC provides a recovery method to deal with timer fault conditions. The following summarizes this method:
Condition 1: The battery voltage is above the recharge threshold and a time-out fault occurs.
Recovery Method: The timer fault will clear when the battery voltage falls below the recharge threshold, and
battery detection will begin. A POR or taking ISET below 40 mV will also clear the fault.
(Question)
1, Why is the BQ24171 designed to clear automatically even if a timer failure occurs?
I think that it is common that the timer fault is cleared by turning on the power again and attaching / detaching the battery.
The BQ24171 is JEITA compliant.
Therefore, is it designed that it is safe to clear timer fault automatically and start recharging?
Could you please answer?
Best regards,
Gk110