Hi,
If I want to set 7.5V of battery charging voltage, what voltage level of Pin CELL_BATPRESZ need to be set?
When I check DS, it shows typical 4 value as below.
But it is not linear when I compared Pin Voltage vs. battery voltage.
Table1. Battery Cell Configuration | |||
CELL COUNT | PIN VOLTAGE w.r.t.VDDA | BATTERY VOLTAGE (REG0x15) | SYSOVP |
4S | 75% | 16.800V | 19.5V |
3S | 55% | 12.592V | 18.5V |
2S | 40% | 8.400V | 12V |
1S | 25% | 4.192V | 5V |
Junghwa