Other Parts Discussed in Thread: BQ25570, MSP430FR5969, BQ25504
Dear TI experts,
I'm doing an RF energy harvesting circuit using BQ25570 for power management, boosting and regulating to supply power to a MCU and different sensors. For BQ25570 to operate, I use 2-stage voltage multiplier (following Karthaus & Fischer's topology) to rectify and initially boost the received AC voltage which is very week (Vpeak = 100mV) to at least 600mVDC.
Without BQ25570, the voltage boosted can reach 1.2V - 1.8VDC. The input power is around 2mW (3dBm) as measured by a spectrum analyzer.
The problem now is, Vout on the EVM can reach only 1.8V, which is not sufficient for the MCU (MSP430FR5969) and sensors to operate. The minimal voltages for these devices to operate are 1.9V and 2.6V, respectively. So, I'm thinking of connecting VSTOR directly to the supply power of these devices.
Could you please suggest any configuration for the EVM to generate enough voltage to these devices? Thank you very much.
P/S: Please place this thread in a more appropriate forum if it does not fit this forum. Thank you.