This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24038: setting of ISET2 pin at AC Mode

Part Number: BQ24038
Other Parts Discussed in Thread: BQ24032A

Dear all,

Could you teach about the setting of ISET2 pin at AC Mode?

I use this device as PSEL=Hi and Iout =1.5A by ISET1 setting.

However, I do not understand about 10.4.4.2 terms.

You mention that 'The charge level for the bq24032A/38, during AC operation only (PSEL = High), can be changed by a factor of 2 by setting the ISET2 pin high (full charge) or low (half charge).'.

Does this mean that Iout will be half of ISET1 when ISET2 is low?

Best regards,