Hi,
I am testing a single cell Li-ion battery with BQ24773EVM. I am using the I2C interface to program the registers. Battery Voltage is 3.685 V and CELL pin is connected to GND. Multimeters are used monitor charging current and battery voltage.
Following are the configuration parameters:
ChargeOption0_MSB (0x01) = 0x81
ChargeOption0_LSB (0x00) = 0x4E
// ChargeVoltage = 4.224 V
ChargeVoltage_LSB (0x0C) = 0x80
ChargeVoltage_MSB (0x0D) = 0x10
// MinVoltage = 3.584 V
MinVoltage_reg (0x0E) = 0x0C
// ChargeCurrent = 960 mA
ChargeCurrent_LSB (0x0A) = 0xC0
ChargeCurrent_MSB (0x0B) = 0x03
I am reading back every register to make sure that all the parameters are set correctly.
When I start the charging process (0x00[0] = 0), multimeter reading for current is 949 mA. However, as battery voltage increases, current starts to drop slowly (1 mA drop per 3 mV gain approx.). Am I missing something here in terms of configuration or setup? All the power-up parameters (CELLS, REGN etc from EVM user's guide) are at expected voltage levels.