Other Parts Discussed in Thread: BQ25703A, BQ25606
Hello team,
I have a customer who has the following requirements:
- The battery chemistry is Li-Ion
- Input voltage is 5 to 5.5V (USB to the solar panel)
- We need to supply 12V to the motor, so we need a boost as well. Since we're a little short on space it will be nice to have a charger with a DC2DC inside
- the current the solar panels provide is 600mA. The USB charger provides 2A. The charger needs to know to work with these voltages and to charge a 10Ah or 20Ah Li-Ion battery pack (18650 in 4 or 6 cell configuration)
the minimum voltage is USB voltage, preferably slightly lower. The maximum voltage should be higher than 5.5V, but other than that is not important.
The charger connects both to a USB charger, and to a solar panel. So if it employs MPPT (maximum solar power) all the better.
can you please advise if this device can be suitable for this kind of application and if you have any other suggestions they are welcome, thanks.
Kind regards,
Shai