Foreign Object Detection (FOD) Calibration/Tuning Tool (Rev. A) (ZIP 60490 KB ) 13 May 2016 |
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Foreign Object Detection (FOD) Calibration/Tuning Tool (Rev. A) (ZIP 60490 KB ) 13 May 2016 |
Dear Bill,
I can download the tool and extract it. Than I have the Installer:
FODCalibration-1.0.1-windows-installer.exe (60,835K)
After this, I do a doubble click to start the Installation. The system asks, whether I want to change the system thru this software and I click "Yes".
Than I see a very short Time the waiting Symbol. After this nothing happens any more. I have no additional Program in the Program list and no new icon. I am the Admin on this computer, so I do not understand the problem, if the installer should work.
Best Regards
Reiner
Dear Bill,
yesterday we got a installation. It seems, the installer is not working on Windows 7. With a Windows 10 system we coudl install it.
It would be good, if you could for the future note the compatibility of the programs on the web page.
Are there any cheaper solutions for the avid components?
Best Regards
Reiner