Hello,
My name is Giang. I am working on battery charger project which is using BQ25101YFPR. It works very well. But in battery absent sate it run with a lot of power (2mA), I think it is too much.
Datasheet shows that:
+ QUIESCENT CURRENT = 1mA in actice mode, =6uA in Iout(done). I try to pull up OUT pin to 4.2V via a resistor 10k to to make the IC go to full charge state when the battery absent but it does not work. How we can go to DONE mode or STDBY mode to save power in battery absent state?
+ BATTERY DETECT ROUTINE run with 2mA IBD-SINK. How we can disable that current in battery absent state?
In schematic, I pull down TS pin to GND via resistor 10k, IN connect to 5V, VSS connect to GND, pull down ISET pin to GND via resistor 2.26k, CHG# pull up via resistor 10k., OUT connect to battery.
Thank you,
Giang