Other Parts Discussed in Thread: BQ25890
I've whittled away the reference diagram from the evaluation board to attempt a minimal schematic for testing purposes. Essentially, I am trying to disable most of the smart features, as this will be in a fixed design with an adequate power supply. Some of the features are not even required, however, I failed to find another option that also had current and voltage reporting via I2C.
I have a crude I2C interface going, setting various parameters. I can see some of the status as follows reported by the IC.
VBUS Status : Adapter (3.25A)
Charging Status : Charging
Power Status : Good
VSYS Status : Not in regulation
Thermal Status : Not in regulation
However, the cell is not charging. The charge current is reporting as between 50mA and 100mA (it varies), but the setting is 512mA. Battery voltage reports 3.7v, so it should be in constant current mode using the full 512mA. Meter is measuring 90mA going to the cell.
Schematic is below.