When I create a Golden ROM file at my location using the "bqTester Software DataFlash Reader, it works fine for me and says file created successfully.
When I send this ROM file to our board supplier for them to program into our boards, they get an error message when using the bqMtester. See attached screenshot. Error message reads: "Single site InitCacheFromSetup() failed for board station1.Error code =65557". This has happens every time I send a ROM file. We are using the bq20zXX series IC's.
It should be noted that I am not using the bqMtester at my location. I am using the bqEval software. The "bqTester Software DataFlash Reader" software being used was part of the Single Station Tester software.
How do I create a ROM file that will work with the bqMtester so our board supplier does not get this error message?
Thanks for your help.