I am yet another user that nhas upgraded my laptop and now need the EV2300 USB drivers for Windowes 7 64 bit please.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Jackie,
It appears that my company's network has stripped the zip file from the email you sent me. I've been told that it most probably will get through if the file extension is changed from zip to something else. Thanks.
Oliver Smith
That did not come through either. Please send to to my home email inspirations@vcweb.org. Thanks. Oliver
Could I also get a copy of the EVM2300 USB drivers for Windows 7 64-bit?
Thanks,
Cliff
Hi Viktoriya,
I would also like the EV2300 USB drivers for Windows 7 64-bit please.
Best Regards,
Flavio
David,
While this driver is only internally tested for now, it has been individually released and we have not seen such a problem yet.
The EV2300 does require you to reinstall the driver each time you switch USB ports. If you are using the same port, I'm not sure why this issue would occur.
Srinivas,
I was not able to send it to that email but check the private message I have sent through this forum.
Regards,
Viktoriya
Hi Viktoriya,
Would you be able to send me the 64-bit drivers (Windows 7) for the EV2300? My email address is herman.law@mysparktech.com
Much appreciated,
Herman
Herman,
Please check the private message I sent to you through the forum.
Regards,
Viktoriya
Viktoriya,
Could you kindly send me the Windows 7 64-bit version of the EV2300 driver to my personal email (company blocks executables): chew@yahoo.com? Thanks.
Regards,
Steven.
Viktoriya Sherman said:Herman,
Please check the private message I sent to you through the forum.
Regards,
Viktoriya
Hi Viktoriya,
today my EV2300 arrived. I'm having the same problem as every guy in this thread...
Win7 in 64 bit version on both of my maschines.
Could you also send the driver via PN or mail to *@*.*? That would be great!
Regards Klaus
P.S.: Excuse my bad english, but I'm from germany and not used to write or speak english very well.
Edit: Got it, thank you! Mail changed.
Can I please get the drivers too (and why the heck do we have to ask for them this way like beggars??? Dont we give TI enough business?).
Thanks.
The unofficial 64-bit drivers for EV2300 are posted in the Files section of the Battery Management forum:
http://e2e.ti.com/support/power_management/battery_management/m/videos__files/458983.aspx
Hi Viktoriya,
I don't know if you are still supporting the EV2300-002 to bq34z110EVM link, but I am having the same problem as the person (Herman) above.
I am using a 64-bit version of Windows7 Professional.
I also get the error "Error E0000235 in UpdateDriverForPlugAndPlayDevices” when I try and load the latest driver.
Any help, such as sending me the driver through a private message would be appreciated.
Sincerely,
Jim 6/27/2013
ps download from the link below
http://e2e.ti.com/support/power_management/battery_management/m/videos__files/458983.aspx
thanks
Onyx
Thanx for your support,but it still won't install this driver, i did execute the file and then when the wizard has finished it says: ready for use.
but when i connect the ev2300 it still says unknown device.
Even when i let it search for the inf files last modefiet and let this file be teh file to install my unknown device it won't work .
Is there also a special manual on how to install drivers for the ev2300 on win7 64 bit ?
sincerely, Alex
HI Alex,
when installing, make sure to install as an administrator and also after installation run the program as an administrator. To do this, click on the right button of your mouse and select the install or run as administrator tab.
Onyx
Hi Onyx,
Thanks for your reply
I did al that, i uninstall the driver install program and reinstall it under administrator, and opend the program bqwizard under administrator.
but still, usb-to-..... not found.
And in the device manager it still say unknown device, when i connect my ev2300
it worked fine under XP so there is nothing wrong with the ev2300
Sincerely, Alex
The link is here:
http://e2e.ti.com/support/power_management/battery_management/m/videos__files/458983.aspx
Remember that this is an unofficial and unsupported driver. EV2400 is the supported option for 64-bit Windows versions. However, this driver will probably work for you.
Hello everybody,
I'm experiencingn the same problem when installing the x64 EV2300 interface driver on Windows 7: even if the setup ends correctly, everytime I connect the devices it's not recognized.
Thanks
Giuseppe
What part are you trying to using ? What message do you see on the screen, i.e. is it definetely the EV2300 driver install that failed, or the EVSW for the EVM you want to talk to i.e. is it not recognising the EV2300 or the EVM. If it does not recognise the part rather than the EV2300, you see a window saying unrecognized part then a list of parts to choose from that does not include your partin which case you haven'y installed correct EVSW for you EVM
To be sure we are on the same page, you should have so far
Did you get this far and it still did not work?
Sorry, I can't get past step 1 "got the Win 7 driver install sw for EV2300 from the link above and installed by right clicking and running as administrator"
Everything runs fine running as administrator or not, but when I plug the usb cable, and go to device manager, the device is still listed as unknown device.
Trying it on a W7 64bit.
Is there a manual way of installing this driver?
Could you please send EV2300 USB Driver for Windows 7 64-bit? On installing the bq evaluation software, it tells me that the "device is not found" whereas the same set up works on other system by installing the driver automatically and detecting the Supercap. Thank you for your support. - Krishna
Need help also on the correct driver for EV2300 for Windows 7 64bit.
Been trying this and cannot make it work.
Always says "Device driver was not successfully loaded"
Please help.