Hi All,
I've been having trouble with operating the GPIO adapter.
I'm working with BQ78PL116 and BQwizard 3.1.
the only way I can read data out of the chip is by sending over I2C through an MCU I programmed.
the BQwizard doesn't work. I flashed the latest firmware for BMS through the USB to GPIO firmware Loader no sucsses, I replaced all wires and connectors, and the driver seems to be installed fine.
the same thing happend with 2 different circuits of BQ78PL116.
I tried also through the BQ78PL1XX API GUI.
I use Windows 7, and the BQwizard have worked before with another adapter
is this a failure in the adapter?
Any thought?
thanks for any help