hello,
I'm going to try and be as specific as possible to avoid some of the misunderstandings I have seen in other questions regarding FETs. Please correct me on any misunderstandings I may have about the operation of the FETs with this eval board.
When discharging or charging batteries (ie, when conducting, when current is flowing through the circuit), the FETs must be closed.
After reaching the max/min voltage programmed in the dataflash, the FETs should open to stop current from moving through circuit. This action should be automatic based on the programming on the chip and the operation of the bq board.
Currently, our FETs can only be controlled manually by using a reset command in bqeasy. Our PRES register is set, and we have no PF registers set.
In addition, once the batteries have been fully discharged (the FD bit in battery status is set), the FETs should open to stop current from leaving the battery. Currently, the FETs are remaining closed, even after the FD bit in battery status is set.
Only by sending the board the default dataflash image can we get the FETs to open, then when we want to close them (to start conducting) we send it a 0x41 word (reset).
Does anyone know why this might be happening and how we can fix it?
Thanks!