Hello
I'm working with the BQ27510 (EVM and on a prototype System), EV2400 and the Gauge Studio.
My System is working so far but I got some basic understanding problems.
- I wrote the Chem ID of my Batt. into the BQ27510 (I can read the correct ID).
But the FullAvailableCapacity still is 1000mAh instead 2900mAh. I thought the Chem ID describes the Batt. with all it's parameters. So whats the Chem Id for?
- If I understood right I should do a learning cycle for my Batt. and write a Golden Image to the BQ27510. How should I proceed to get the correct Batt. parameters into the BQ27510? Can I do this with the Gauge Studio?
- What are the main steps I need to do that I get the correct parameters out of my Batt.?
Thanks in advance for every help getting me a better basic understanding.
Greets Gerald