Hi,
we will use the bq40z50 for an 2-Cell Li-Ion battery pack in an microcontroller driven device.
I've read the thread "Introduction to Multi-Cell Gas Gauges" on top of this forum and some other articles here.
Is it absolutly necessary to flash the device with bqStudio - or can i setup the parameters as an "initialization-sequence" from the microcontroller?
The default configuration for the bq40z50 i've seen is an 4-Cell-Pack.
Which minimum steps i have to do to configure the bq40z50 for an 2-Cell-Pack?
I've setted up the DesignVoltage() and DesignCapacity().
What i must do that i can charge and discharge the pack?
The IC goes to Sleep or something else after 5 Seconds - then it does not respond to any SMBus-Command. I toggled the LEDs on with "ManufacturerAccess() 0x002B LED TOGGLE" and they go off after this timeout.
Dirk