Hello,
I would like to send in a LEOCH LP12-18 battery to be Characterize for a project we are working on with the BQ34z110.
What information on the process can you provide?
Also I have seen from an earlier post that There is a bug in the released FW that will not allow the Passed Charge to increment above 16383 mAh. It mentioned 'will need to use 2x scaling' is that the same or different than setting the X10 bit on?
Any information you can pass along would be great.
Regards,
Ron