This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Christophe,
Can you share what procedure you followed to configure the gauge? What chemID are you using with the gauge and how did you select it?
Are you really using it at -30degC? That will be a challenge for gauging because the cell resistance goes up incredibly quickly at sub-zero temperatures, and can also vary a lot from cell to cell.
Hi,
I use bq Evaulation Software v0.9.92 to configure with bq Easy. Our battery is NCR18650PF from Panasonic then i select ID 0x2020 with bq Easy. But we don't acheive bq Easy learning cycle correctly,it always fails then we do it manually because automatic cycle doesn't work with EV2300.
Our application need to work between -30degC to +60degC, i test battery and EVM27510-G3 really at -30°C in Temperature environmental test chamber.
I do the same test with another battery at -30°C and i have same result.
Our application need to have a good precision (>=2%) at sub-zero temperatures.
Is bq27510 adapted to this condition ? how can i be sure that our settings are good ? have i forgotten something ? is a parameter wrong ?
Thank you for your help !
Hi Christophe,
We would need to optimize the battery profile for your battery at such an extreme temperature. Most of our profiles are created for 0C to 50C accuracy.