I am trying to change the calibration values in bq27510-G2 using the bqEVSW flash tab. I can write the Pack V Offset and temperature, but not the CC Offset value. The data field becomes red and an Error message is shown: "The value entered is out of limits. Please enter a value between -2.411 and 2.411 mV.
The value I try to enter is -0.104 which is within this range. Even if I just click in the data field and press enter to accept the default value, I get this message. If I enter an integer, there is no error message, but the value will still not be written to the flash.
I am using bq2751-G2 version 1.23 and EVSW version 0.9.92.
I have disabled SLEEP (Op config=0959). IT Enable=0 and Update Status=0.
Flash Update OK Voltage is ok.
Do you have some advice to give on how to solve this?