NR is set
Current Recovery Time is 8s
AFE OC DSG is 0x00 (4.5A in my circuit)
AFE SC DSG Cfg is 0x70 (9.1A in my circuit)
If I set the load for 4.6A, AOCD goes up for 8s, then goes back down. If the load is still on, the flag goes up again immediately. This is expected behavior. If I turn the load off, the flag resets and stays off.
If I set the load to 9.2A, SCD goes up, but after 8s it is still up. It will not clear itself with the timer. It should, because NR is set, and SCD is supposed to behave just like AOCD in that it resets with the timer.
Average current is -3mA. in both cases.
???