Hello!
I use a 12s2p 10.2Ah lipo battery with 50400mV (12*4200mV)
maximum voltage. I have to define it chemistry ID because "E-
Stars 1143128 5100mAh" cell isn't present in Chemistry selection
table. I don't use evaluation board, so Evaluation Software too.
According to this forum, I can define chemID by using
"Identifying unknown chemistry simple discharge test – 24 hrs"
or your help, BUT bq34z100 measures Voltage of the pack not
properly.
My Rseries=976k with bottom R=16.5k and parameter of the Voltage
divider was 50400mV.
First, I thought the problem is in Rseries and I changed
parameter of the Voltage divider to 54136mV to reach 900mV, but
bq34z100 measures Voltage not properly again.So the question is:
what isn't right with Voltage measuring in my case?
And the second question, what would happen with all of this
calibrations, SOC, RM etc. if power of bq34z100 will be switched
off?
Thanks a lot