Hello,
I have made a Golden file, loaded it into several packs, calibrated them and enabled the IT algorithm. These packs now have Update Status: 6, but Max Error 143%. I understand (from other posts), that this is due to a mismatch between cycle count and the corresponding hidden constant version of cycle count. Thinking back to when I produced the golden file, item 5, 11.3 pg 209 SLUA404 says 'Write a .senc file with the correct chemical ID to clear the hidden data-flash constants". At this stage, I used bqEVSW 0.9.86/bqEasy/4.Chemistry/4B. Select Chemistry Manually/ to (re)write the chemistry file. Perhaps I should have instead used bqEVSW 0.9.86/bqEasy/Pro/Srec Programming, or do they both clear the hidden constants? When will Max Error fall to 1%? Is it after relax (5hours), discharge a little, relax (5 hours), or is there a faster way?
Thank you,
Jeremy.