Hello.
Background:
I am using the BQ27421-G1 for a system-side battery gas gauge which will connect to removable battery packs.
Question:
1) When I switch battery packs, how does the gauge accurately measure the state of health?
2) Does it take a full discharge cycle or some amount of time?
3) I can plug a 100 mOhm resistor in series with the battery pack to simulate aging and the state of health does not change more than just a few percentage points, is there a more appropriate value to use, or does it take a specified amount of time to update this value? We saw about a full discharge cycle to drop 2-3%