After experimenting with the kit/reading the manual I got one more question:
In the bq27530-G1 TRM (SLUUA73) references are made to registers Chrgr_InCtrl_Reg0, Chrgr_POR_Config_Reg1 and so on (see pages 22 to 28 in the TRM). How do these register/messages relate to the Flags / Status Bits shown in the bqEVSW's DataRAM page?
Example:
bqEVSW DataRAM shows Chrgr_Ctl_Stat_Reg0 --> is this the same as TRM, page 22, Chrgr_InCtrl_Reg0 ???
bqEVSW DataRAM shows Chrgr_Supply_Stat_Reg1 --> TRM, ?????
Thx
MH