HI,
Iam new to fuel gauge monitoring .. i need to design battery charger + monitoring circuit for handheld product.
With help of TI FAE , i have narrow down following part for my application. with basic view of datasheets i drafted block level for battery charger + fuelguage
monitoring circuit.
Input Specification:
Li-ion : 3.7v / 2200mA (4S) = 14.8v
Input : 15V DC Adaptor
i have following question
1. Concept diagram is ok ?
2. what are the parameter i need to look for before start evalution?
3. part no selected is ok ? since as per bqz2045 evm using cell balancing bq29412
which NRND so we selected bq 7718xy..
4.Any other parameter i need to look ? for both charger and fuelgauge.
Regards
Anbu UB