Hello,
i will change the Cell Voltage Threshold from 2500mV to 3000mV. For this i take the example from the Datasheet SLUU513 (September 2011).
If the voltage drops below 3000mV the BQ28550 closed the connection to the battery - that is fine.
But if i connect the System with powersupply - nothing happens.
If i send the QB28550 over i2c the shutdown command the BQ28550 closed the connection to the batteryand it starts with connection to powersupply.
Why start the system by using the shutdown command and not with the Cell Voltage Threshold?
Best regards
Rene