Hello, Thomas,
I have started lately with a brand new BQ40Z60EVM-578. The PCB has a label Rev A on it, the firmware is v0_13_build19. The pack is 2s LiPol 9.7Ah, learning cycle fulfilled successfuly.
My problem is: for some reason the charger characteristic isn't flat enough in the constant voltage region and the pack voltage tends to rise in excess of 300mV over the programmed level. Actually I never allowed the charger to fully complete the cycle with initial settings even as low as 4075mV for fear to drive the pack overcharged. I can accomplish charging with FC and no heartache only by issuing several tiny manual voltage corrections in the course of it. Luckily these data flash writes have an immediate effect. Please help me make charging controllable. I attach zip with registers and data flash contents (hope I did it right;-)
Please let me also ask for some clarifications, regarding Technical Reference Manual sluua04:
- CHG_FET bit mentioned at p.63,68 is missing from FET Options table p.153, but shows in bqStudio
- CHGIN bit mentioned at p.68-69 is missing from both FET Options table p.153 and bqStudio
- No formulae for calculation nor definition of LCHG Current Resolution
- PCHG_COMM bit mentioned at p.67 is not found elsewhere
- ChargingConfiguration[LCHGM] function needs clarification
- PF Shutdown Voltage/Time at p.75 - no definition found
- IT Gauging 2 Configuration at p.153 - no definition found
- initially BTP_INT bit was stuck set despite of BTPCharge/DischargeSet() commads, but it changed at some point and now the commands have effect - what can keep the bit from clearing?
- does BTP pin reflect only configured BTPCharge/DischargeSet() events and no others? (I'm a bit confused with a pin name ALERT in datasheet.) Can a slight pull-up be switched off from the pin?
And at last I report a slight (at room temperature) influence of LED display on temperature measurement in EVM: 1uF capacitors and 330kOhm resistors give about 2K swing as the LEDs blink. I removed the capacitors from EVM and try to ignore the resulting visual effect.
Thank you very much.
Sergey