Hi,
I am currently looking at the user guide named SLUUB71–November 2014, depending battery management (the file is attached)
The circuit diagram in figure 17 respectively the bill of materials in table 6 show two diffent types of 10µF capacitors. One is designed for 35V and the other one for 50V. Now I am wondering why there are used two different types? Would it not be possible to use just the one desgined for 35V for all four 10µF capacitors ? If not, what is the specific reason for that ?
Nermin