Hello,
Design Voltage
In the Battery Management Studio 1.3.40, in the Data Memory tab, class configuration->Data, there is parameter named Design Voltage, which has a default value of 3600.
In the TRM this value does not exsist, it should have been in Data->Subclass ID 48.
Do I need to change this value, I would think it should have been 3700?
Design energy/ Design Capacity
The charger charges only to 4100 mV in my system, to extend the lifetime of the battery. My battery is marked 3850mAh.
Do I then set Design Capacity to 3850 * 0,9 = 3465?
And then use the 3465 in the calulation of Design Energy ( 3465 * 3,7 = 12820)?
Best regards,
Frank Andersen