Dear. All.
I have one issue about FD(Fully discharged) set issue.
i using BQ28400 with Li-polymer 7.4V 12.5Ah.
Parameter for FD.
1. Configuration (Subclass 146)
Full Discharge Set % (Offset 2) : 2%
Full Discharge Clear % (Offset 3) : 5%
I tested 0.2C(2.5A) discharge.
When RSOC is 2%, FD didn't set.
When RSOC is 0%, FD didn't set.
When TDA is set, FD is set.
I cannot found FD set point.
Please help me.
Thank you.