Hello,
I am performing the learning cycle on a 110Ah, 12V, AGM battery and have a few questions:
1. Recommended charge rate is C/2. My charger maxes out at 15A (between C/5 and C/10). Besides taking a long time, will this be a problem?
2. Taper current is recommended to be between C/20 and C/10. In may case this would be ~7A. In the Taper Current field in DF, should this be entered as 7000[mA] or as 700[cA]? I have X10 set high.
3. What is an appropriate Min Taper Capacity? I have the Current Taper Window set to 40s.
4. Appropriate setting for Cell Taper Voltage?
Thanks for the help.
Fernando