Dear all,
we are using a circuit based on BQ40Z50 IC.
we are going to production stage and we need to have 3 calibration stations to burn and test these boards.
I saw that TI has a very nice flow with the BQproduction SW and environment.
please clear this issue for us, could not understand it from the Advanced bqMtester:
in order to implement 3 stations I need:
- computer with BQproduction SBB software on it.
- 3 x USB inputs on the computer / USB hub.
- 3 x EV2300 / EV2400.
- 3 x ADVANCED-BQMTESTER.
- external power supply 24V and 5V.
is the ADVANCED-BQMTESTER is actually the HPA495?
if so that what you would call a CAL board in the user guide flow (sluu397a page 6)?
is there a smarter way to establish these stations?
we need:
- srec file burning
- current, voltage, temperature calibration
- S/N - ing
- log file
many thanks,