Hello
I have some issues with the firmware update of an bq40z50. I did the learning cycle and export the Srec-file in order to update another 40 samples.
I select the Srec-file (which is located on a server) and push "Program" button in bqStudio (Execute after programming was checked).
This works fine for the first three samples. At the fourth sample the update process stopped after a short time. From then on the sample is not longer reachable. bqStudio reports two errors:
1. No acknowledge from device (this error is displayed all time)
2. Packet checksum mismatch (this error is displayed only a few milliseconds)
The next 3 samples got the same issue.
I suspect, bad network connection while downloading the Srec-file from the server is responsible for the issue. Can anyone provide detailed information about the firmware update process?
Is there any possibility to reanimate the 3 broken samples? Maybe a kind of hard reset?
Thanks
Patrick