After trying to set the charging voltage for a 2S2P to 8400mV to within 100mV (50mV per cell) doesn't seem likely without some type of trimming. Adding up worst case using 1% resistors and the 2% VFB tolerance this could add up to almost 4% around 300mV on 8400. Please someone show me I'm wrong, or an easy way to trim it.
The second problem the FB network on the EVM using 1% resistors can exceed the 12200 mV limint using 4200mV cells. This can be 1235mV in my case and I will need to change them to prevent this..