In the document sluub71 page 4 it shows that there is a system load between VSYS and PGND. If we are testing the charger with the EVM2300 is it required to have a system drawing power as well? It seems like the bq40z60evm and the evm2300 are enough to allow the software to work, but I'm not sure if I'm supposed to place a fake load here to simulate a system drawing power or if I can just leave it disconnected.