If we are forced to use more than one battery management IC in our pack because we must balance charge in parallel cells, is it possible to combine the SMBus lines of two or more Battery Management Units, like bq40z60 and address each individually?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If we are forced to use more than one battery management IC in our pack because we must balance charge in parallel cells, is it possible to combine the SMBus lines of two or more Battery Management Units, like bq40z60 and address each individually?
Mark,
You can have three independent packs with a bq40z60 device in each pack. The packs can be connected in parallel with the PGND signals (on the J1 connector on the bq406z60EVM schematic) connected together. The VSYS signals could be connected together, but this would result in the packs being able to charge one another in an uncontrolled manner. You can prevent this by adding a series schottky diode to each VSYS output (J5 connector) and connecting the cathodes together and to the load. This will prevent reverse current and charging one another. The VAC signals can be connected together to charge the packs.
Does this sound reasonable?
Tom
Sounds reasonable. Do you have component suggestions for the SMBus multiplexer?
Thanks,
Mark