I am down to what I hope is my last problem in using the bq27425 Fuel Gauge chip. The problem is that I do not get usable values in response to the commands that relate to the battery capacity. Specifically, I get zero (0) for
NominalAvailableCapacity 0x08/0x09,
FullAvailableCapacity 0x0A/0x0B,
RemainingCapacity 0x0C/0x0D, and
FullChargeCapacity 0x0E/0x0F.
And most troubling of all I get 0 (zero) as the value for
StateOfCharge during the first 5 minutes of inquiry (if the battery is charging) and then I get 100% forever after.
In addition, I get 0 (zero) for all inquiries of StateOfCharge always if the battery is discharging when connected to a load without being simultaneously charged.
Furthermore the StateOfHealth 0x20/0x21 always reads 0x100 (even though the spec claims that its max is 0x64)
I am having so many problems related to reading the battery that I feel that I need to speak directly to an expert. I have tried putting my questions on the E2E bulletin board before, but I do not get the help I need. Can I please get connected to an expert.
I am Richard Brisk a design engineer at Kopin Corp.
The phone at my desk is (508) 870-5959 x117
My personal cell phone is (774) 270-0093
My email is RBrisk@Kopin.com
Please call or write with information as to how I can connect with an expert directly.
Thank you,
Richard Brisk