I have been going in circles for the last few days trying to configure the bq40z50 for my test application. I thought I had the correct battery chemistry, but I am getting a R_DIS flag during the learning cycle which according to SLUA597[http://www.ti.com/lit/an/slua597/slua597.pdf] indicates that I have an incorrect cell chemistry selected. I want to use the battery management chip with a LiPo battery and it seems that the default ChemID of 0x0100 is not correct.
I was hoping to perform a chemistry learning cycle (as is described for the bq20 and bq30 chips), but I the bqEVSW software doesn't recognise the BQ40Z50. It complains that it requires an .encr file.
Up until now I have been using bqStudio to configure the chip, but it does not have the facility to perform a chemistry learning cycle, hence why I tried using the older bqEVSW.
I am using an EV2300 to communicate with the bq40z50.
I have also attached the .srec file, if that may be helpful.
How do I perform a chemistry learning cycle for the bq40z50?
Thanks for the help.