Hello,
I have a problem with the Gas gauge BQ34Z100-G1 while working with Pba EFB 70Ah battery (Varta E45):
while leaving the battery for rest the BQ34Z100-G1 resets its values and think that the battery SOC is 100%,
For example: The battery was 100%, I discharged it to 66%, I did let the battery rest and after about 40 minuts the gauge reseted its FCC,True RC and SOC value.
The log for the test is attached here, can anyone please help me understand whats causes the gauge to resets it's values?
It happens in sample number 5762.
2654.afterOCVwhileDischarging.log
Regards,
Shlomy