Hi,
We are trying to calibrate bq34z100-g1 for non-rechargeable Li-ion cells. We are using 2 cells in series. Can anybody help with the calibration steps we need to do without using evaluation tool?
About the Li-ion cell:
- capacity: 1550mAh
- voltage: 3v per cell.
I have updated the following parameters:
- voltsel bit to 1
- design capacity to 1550mAh
- design energy to 9300mW
- number of series cells: 2
- flsh update ok cell volt = 3888
How can we run the learning cycle so that the fuel gauge reports the remaining capacity correctly?
Which steps are required to fully configure and calibrate the fuel gauge for non-rechargeable cells without using the evaluation tool?