NiMH.zipHi,
I'm trying to perform an optimisation cycle with a battery pack NiMH. All the flags seems to change correctly but the update status remains at 4, the Max error remains at 100% and cycle count doesn't increase (still at 0).
Hereby i took printscreens of the Registers during the optimisation cycle. The optimisation cycle I used is:
- charge to 100% (C)
- Relax > 5h
- discharge (C/5)
- Relax > 5h
Do you have an idea why the Max error remains at 100% and the update status remains at 4?
Thanks,
Pierre