Hi TI Experts:
For the BQ27510-G3 fuel gauge, I understand that it need to configure the battery nominal capaity and other parameter.
What if I didn’t configure, it is fuel guage will able to detect my battery level in default condition??
I have try to connect Li-ion battery to bq27510-g3 directly using default condition and charging.
But the bettery level shown at bqstudio just remain.
Sometimes, the battery level dropped when the battery is still charging.
My Li-ion battery capacity is 1000mAh.
If we do not configure any parameter on the bq27510-g3, what reading that we suppose to obtain?
Please advice,
Wang
Please advice.