I've been trying to install the EV2300 driver on to my system without any success. My system is XP Professional x64 Edition, with Service Pack 2. I have admin rights on my computer. I've tried to install it 2 different ways, through the instructions listed with the downloaded driver (in the folder /documentation/Files/FirstInstall) and also through the way documented in the SLUA352A.pdf. Both of them give me the same error, after I accept that the drivers haven't been tested on Windows 2003 and hit continue, and then I agree to the license agreement, I get the following error: "Error E0000235 in UpdateDriverForPlugAndPlayDevices", and of course the installation does not complete sucessfully.
Is the EV2300 compatible with XP x64? What else do I need to do?