We have a 1S3P Li-Ion pack using the bq40z50-R1. Pack has gone through a learn cycle and Update Status register is 0x0E so both the QMax and Ra tables have been updated.
During a C/20 discharge the RSOC stays at 100% for the first 2 1/2 hours before moving. At that time the actual capacity is down to about 88%. Is this expected behaviour? Is there any way to adjust?
The chart below shows a constant current discharge at 270mA. The Cap line represents actual capacity as a percentage of the measured capacity during the discharge to 3.1V
Thanks,
Greg