We used the TI BQ27421 gauge in the project.
1) The value of AverageCurrent( ) Standard Command (0x10 and 0x11) is always 0.
1-1) So, the gauge enters the SLEEP mode because the AverageCurrent() < Sleep Current.
2) The test conditions
2-1) The gauge is on the I2C-bus.
2-2) Because the calibration of the battery is not completed, we downloaded the example of flash stream file into the gauge.
2-2-1) The example of flash stream file does not meet the requirement of the battery in the project.
2-2-1-1) For examples: Design Capacity is 1340 mAh in the flash stream file. But the battery is 9600 mAh.
2-3) The Sleep Current (Subclas 82, offset 31) are set to 10.
Q-3) Is the value of AverageCurrent() always 0 because the flash stream file (without battery calibration) is incorrect for the battery?
Thank you.