Hello,
I was reading through the TRM for the BQ28Z610 gas gauge and I came across a section that talks about the Full Charge Capacity (FCC) and the maximum chemical capacity (Qmax). These are my understanding of the two parameters:
Qmax: the maximum chemical capacity of the battery pack.
FCC: the amount of charge passed from a fully charged state until the battery reaches its termination voltage. (It seems that the value calculated for FCC would equate to the Qmax)
To me it sounds like the parameters are referring to the same thing if not extremely close, and I want to be able to differentiate when the TRM mentions them. Could you clarify or correct me if I am mistaken on what these refer to?
Thank you for your time.
Blake