Hi TI members,
My customer said sometimes write failure was occured when he writes DFFS file data to bq27520-G4.
It seems bq27520-G4 was still in the state of "ROM mode" in this case.
He added the following "Exit ROM mode procedure" when the write failure was occured, then he achieved to exit "ROM mode".
--------------------------------
W: 16 00 0F
W: 16 64 0F 00
--------------------------------
However he repeated above rewrite sequence several times, bq27520 eventually forces SCL low level as the following and doesn't release SCL until powering off.
Once it occures, bq27520 inevitably forces SCL low level again in next rewrite sequence although after powering cycles...
In other words, I2C master can't access bq27520 (address 0x55) from then on.
.
Do you have same experience with bq27520-G4?
Is there any workaround?
Best Regards,
Yaita / Japan disty