Hi,
I am using bq27441-G1A with MSP430 controller. I want to update the design capacity parameter to 750mAh of bq27441-G1A. I have implemented the flow given in TRM but when i read the design capacity with "DesignCapacity(): 0x3C and 0x3D" , It shows default value 1340 instead of 750. Is there any other changes i need to do to update design capacity parameter?