I have been trying unsuccessfully to get the BQ34z100-g1 to go closed loop and get beyond learning state 4 in activating the Impedance tracking.
I was wondering if a TI employee could look at the log files and see what might be the issue. It reports measuring the OCV at charge and discharge but the max error remains at 100% and QMAX never updates too. The SLUA334B document and others like it imply that max error should go to 3% on the first charging cycle and I do not see that happening. The QEN and VOK bits seem to do what the document says they should be doing when doing an optimization cycle. The SOC matches well when charging and discharging the QMAX value used, so that seems correct. I read in some of the documents that starting it from a discharged state and issuing a reset is helpful, so that was done. The battery is a Pb 12 Volt battery.
The first indication seems to be in the charging cycle when MaxError is supposed to go to 5%.